REC.GAP

Description

REC.GAP specifies the gap between consecutive samples. The recording base rate is 16 kHz, thus a gap of 1 means that a sample is recorded every 62.5 µs.

Examples

Code

To record data every 125 us:

-->REC.GAP 2

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 65,535

Default Value

1

Data Type

Integer

See Also

REC.TRIG

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.